Part Number: THVD1550
Dear all,
I have a question for THVD1550
It uses in the form of the following circuit diagram and communicates without using the terminating resistor
At that time, when the output signal of RS-485 was confirmed, it was found that the waveform became dull in the case of H output as shown in the waveform below. (Part surrounded by a red dotted line)
I believe that this phenomenon is caused by a change in voltage as shown in the graph below due to a change in output drive current. Therefore, it is considered that this phenomenon can be solved by connecting the terminating resistor to the output.
However, when the above is a factor, it is thought that the shape of the L output is also dull as in the case of the H output, but there is no dull shape like the blue dotted line portion of the waveform .
I would like to ask if there is any problem with the phenomena currently seen in the waveform that I am considering.
Best Regards,
Y.Ottey