This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP159: What's the connection on HDMI connector pin 13, 14? CEC and SPDIF_IN

Part Number: SN75DP159

Hi expert,

My customer would like to know the connection should be on HDMI connector pin 13, 14 and what does these do for?

Pin 13 CEC

Pin 14 SPDIF_IN

  • Hi

    For CEC, please refer to Fig 30 of the DP159 datasheet. CEC is connected directly from pin 13 of the connector to the source assuming this is a motherboard design.

    DP159 does not support ARC (audio return channel) function, the SPDIF connection will be between the source and the connector, bypassing DP159.

    Thanks

    David