Part Number: XIO2001
Hello,
I have a design with XIO2001 which I have designed based on TI's EVM board and I a have power-up issue with my board:
Since i need it as a simple PCIe To PCI bridge, i do not use a EPROM to configure the device. Based on the EVM board ("Pin 9 on the J1 header is a global reset (GRST ) for the XIO2001. Driving this pin low will cause all registers and state machines within the XIO2001 to return to a default power-up state. This pin generally must remain disconnected.") and based on the implementation guide :("During an XIO2001 device power-up from the D3cold power state, there is no requirement to assert this terminal low"), i have left GRST pin floating.
While turning on the PC, it's seems that the PC freezes. The PERSTN signal goes from low to high while turning on the PC. If I am asserting and deasserting (gnd to 3.3V) the PERSTN signal manually then, the PC continues with it's boot, but in device manager the bridge comes up with code 12. I have tried it on several PCs.
I have also tried to add some delay to the PERSTN signal, with no change.
I have tried some of the solutions in the support forums with no success.
Please advise,
Regards,
Yossy Goldenberg