This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: Whether I could read 948's status(PDB/LOCK/PASS) through 947 without MCU and GPIO

Part Number: DS90UB948-Q1


Hi Team,

My customer don't want to add MCU in 948 side in order to cost down. And GPIO[0:3] are also used.

Without MCU in 948 side, is it possible to read 948's status (PDB/LOCK/PASS) through 947?

The question can also be described as how to read 948's PDB/LOCK/ Pass status through 947, since 948 has no external MCU?

  • Hello Amelie,

    If the SER/DES pair is unlocked then you would not be able to read anything through the back channel. That goes for LOCK and PASS. PDB is a reset for the device so if PDB is low then the device will not function at all either. 

    Best Regards,

    Casey