Part Number: DS90UB953-Q1
Hi Team,
In my project, 954/953 connected with coax and using POC.
Configured as non-sync internal clock mode.
954 configuration:
WriteI2C(0x4C,0x01)
WriteI2C(0x58,0x5A)
WriteI2C(0x4C,0x01)
WriteI2C(0x5C,0x18) #953 ID alias
WriteI2C(0x5D,0x34) #Sensor ID
WriteI2C(0x65,0x1A) #Sensor ID alias
WriteI2C(0x6D,0x7C)
WriteI2C(0x0C,0x81)
WriteI2C(0x1F,0x02)
WriteI2C(0x33,0x03)
WriteI2C(0x20,0x20)
953 configuration:
WriteI2C(0x02,0x73)
WriteI2C(0x05,0x0B)
WriteI2C(0x0E,0xF0)
WriteI2C(0x0D,0x0F)
My questions:
- The REFCLK_VALID bit in 954 DEVICE_STS(0x04) register is 0.
Is it correct in non-sync internal clock mode? - The COAX_MODE bit in 954 PORT_CONFIG(0x6D) register is 0.
Should I set it to 1 in configuration? - After writing configuration to 954/953, there is no error in 954 CSI_RX_STS(0x7A) register.
But it doesn't receive any thing from sensor. Does it have any missing configuration?
Thanks!