Part Number: PCA9306
When the SCL1, SDA1, SCL2, and SDA2 lines are low, there is a step of about 0.7V.
What should I do to lower the Low level below 0.6V?
The pull-up resistance of I2C master side(1.8V) and slave side(3.3V) uses 10kΩ.
What should I do to lower the Low level below 0.6V?
The pull-up resistance of I2C master side(1.8V) and slave side(3.3V) uses 10kΩ.
I hope you get a reply.