This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IR: Interrupt output setting

Part Number: DP83867IR

Hello team,

My customer would like to configure INT/PWDN pin as interrupt output.

They wrote "1" to INT_OE(7-bit of CFG3). However when they read back the register the bit remain "0".

Is there any restriction on changing the bit to "1"?

Best regards,

  • Hello Taketo,

    There is no restriction on changing the interrupt output enable bit. Can you please provide the full register read/write commands you are using? Is the part being reset between setting and reading back the bit?

    Regards,

    Justin