Part Number: TCA9406
Other Parts Discussed in Thread: PCA9306,
Hi,
I`m searching a I2C levelshifter from 1,95V to 5V Logic. I have found that two guys but I dont see the huge difference between them. Ok one has internal pullups what is good to have.
2ndly I have to ask what happens in the following case: VCCA is 1,95V. VCCB is 5V. What happens if the logic high on the A-Side is only 1,8V? Are there any high cross currents what I have to consider?
Thanks & best regards,
Markus