Part Number: DS90UB935-Q1
Hello,
It may be a basic question, but allow me to ask that regarding Mipi data rate.
We can find the following description on the datasheet. (at 6.3 Recommended Operating Conditions)
- Mipi data rate (per CSI-2 lane): up to 832Mbps max
- Mipi combined data rate: up to 2.5Gbps
Does the Mipi combined data rate mean 4 lane aggregation? (625Mbps x4)
Thanks in advance.
S.Sawamoto