Part Number: PCA9306
Other Parts Discussed in Thread: TXS0102,
Hi all,
I have an application in which I need to convert the Level of I2C bus of GSM module which is working on 2.8V to 3.3V.
I have 2.8V/20mA and 3.3V/150mA available onboard for Supply Purposes.
I am not sure whether this IC supports the above translation?
If not then please suggest which IC support this translation between 2.8V - 3.3V for I2C bus.
Can I use the TXS0102 part for this?