Part Number: TPS65987D
Other Parts Discussed in Thread: TPS25740, TIDA-050012
Team,
A customer of mine woule like to use a GPIO to select the max power that TPS65987D is delivering to a connected USB device. I only found the option to create two different configurations which seperate supply voltages and currents (register 0x32), but not with a power limit.
How can a max power limit be selected? This feature is available on TPS25740 via the PCTRL pin.
Background of the question: there is one big power supply which supplies multiple TPS65987D. Each TPS acts as charger for a conntec USB device. And the power supply tells the TPS via a GPIO if it is allowed to draw 60W or 30W.
Thanks,
Robert