This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: DS90UB954-Q1: CSI- Bandwidth

Part Number: DS90UB954-Q1

We have got sensors (such as  OmniVision OX03A10 FHD 1920x1080) with four CSI-2 lanes and a data rate of about 2.1 Gbps.

I used UB953 to test that the above sensor uses four CSI-2 lanes.

When the UB954 can be changed to use two CSI-2 channels to transmit, the data rate is the same as 2.1Gbps.

Whether such an architecture can be achieved and how to set it?