This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ONET1141L: ONET1141L with grounded anode laser

Part Number: ONET1141L

Is it possible to use the ONET1141L to bias a grounded anode laser?

The laser for my project has the chassis connected to the laser anode and a K connector for the modulation input. I would like to keep the anode/chassis grounded so I can interface with the K connector without worrying about shorting anything.

I was thinking about trying to use the ONET1141L with Vcc = 0 and GND = -3.3 V and set BIASPOL = 1 to sink current.