Part Number: TPS65988
Other Parts Discussed in Thread: BQ25703A, , BQ4050, TPS65987D
Hello,
I have a design based on TIDA01515 with TPS65988 / BQ25703A and BQ4050.
I manage to configure BQ4050 by I2C to work correctly. I then went to the TPS65988.
Currently USB2 output is working and charging devices I plug on it. I got events on USB C insertion and I can see the kind of power adapter I'm using.
However I can't manage to make BQ25703A work with the TPS65988. I followed the slvae18 recommendations (except for the GPIO EN_OTG which is not described).
I also tried the 5545.88DH Power Bank.pjt one of TI experts posted on this forum.
Nothing works. I need to add that PP1 switch is enabled and I see the right voltage on the BQ25703A input.
Could you help me find a way to check if I2C is OK between the two chips ? In debug mode maybe ?
Best regards,
Michaël