This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDP158: Differential pairs on pinout description is unclear.

Part Number: TDP158

Hi,

I don't understand why the pinout description stated both PLUS and MINUS signals for each pins of differential inputs and outputs of the TDP158 (datasheet page 4). For example, both pins 1 and 2 are named: "IN_D2p/n". The lane inversion does not seem to allow PLUS and MINUS swap anyway.

On figure 42 (page 39), the pinout is different: now PIN 1 = IN_D2p and PIN 2 = IN_D2n.

Can you confirm what is the correct pinout?

Thanks,

Denis Alain, Eng.