Part Number: SN65DP159
We are evaluating a prototype board equipped with SN65DP159, but the output is not recognized properly.
Symptoms: HDMI signal does not appear ( 'Signal Error' is displayed on the monitor, but only the signal frequencies are recognized )
Signal: 3840x2160 59.94Hz
Monitor: EIZO EV2785
We use this device on the products, so we designs according to past design data. Something is wrong but we can not find it.
We found that especially the DC level of TX2+ is very low, and we think this may be the cause.( Please refer to the attached file. )
Do you know why this happens?
/cfs-file/__key/communityserver-discussions-components-files/138/SN65DP159_5F00_TX.xlsx