Part Number: DS90UH949-Q1
Other Parts Discussed in Thread: DS90UH940-Q1
Hi
We are using DS90UH949-Q1 and DS90UH940-Q1 as a pair to send HDMI signal to the processor.
When doing HDMI plug test, around every 50 times we will see one failure that video disappear
Two symptom may appear
Symptom 1. DS90UH949-Q1 did not detect the HDMI clock the DS90UH949-Q1
[REGISTERS] Device = ALP Nano 1 - DS90UH940, Connector 1 Comments = "1234" Date = 04/06/2020 Time = 16:47:59 Reg = 0,0x0000,0x00 Reg = 0,0x0001,0x00 Reg = 0,0x0002,0x00 Reg = 0,0x0003,0x00 Reg = 0,0x0004,0x00 Reg = 0,0x0005,0x00 Reg = 0,0x0006,0x00 Reg = 0,0x0007,0x00 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x00 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x00 Reg = 0,0x000D,0x00 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x00 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x00 Reg = 0,0x0016,0x00 Reg = 0,0x0017,0x00 Reg = 0,0x0018,0x00 Reg = 0,0x0019,0x00 Reg = 0,0x001A,0x00 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x00 Reg = 0,0x001D,0x00 Reg = 0,0x001E,0x00 Reg = 0,0x001F,0x00 Reg = 0,0x0020,0x00 Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x00 Reg = 0,0x0023,0x00 Reg = 0,0x0024,0x00 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x00 Reg = 0,0x0027,0x00 Reg = 0,0x0028,0x00 Reg = 0,0x0029,0x00 Reg = 0,0x002A,0x00 Reg = 0,0x002B,0x00 Reg = 0,0x002C,0x00 Reg = 0,0x002D,0x00 Reg = 0,0x002E,0x00 Reg = 0,0x002F,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x00 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x00 Reg = 0,0x003D,0x00 Reg = 0,0x003E,0x00 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x00 Reg = 0,0x0041,0x00 Reg = 0,0x0042,0x00 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x00 Reg = 0,0x0045,0x00 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x00 Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x00 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x00 Reg = 0,0x0051,0x00 Reg = 0,0x0052,0x00 Reg = 0,0x0053,0x00 Reg = 0,0x0054,0x00 Reg = 0,0x0055,0x00 Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0059,0x00 Reg = 0,0x005A,0x00 Reg = 0,0x005B,0x00 Reg = 0,0x005C,0x00 Reg = 0,0x005D,0x00 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x00 Reg = 0,0x0061,0x00 Reg = 0,0x0062,0x00 Reg = 0,0x0063,0x00 Reg = 0,0x0064,0x00 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x006D,0x00 Reg = 0,0x006E,0x00 Reg = 0,0x006F,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x00 Reg = 0,0x0074,0x00 Reg = 0,0x0075,0x00 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x00 Reg = 0,0x0080,0x00 Reg = 0,0x0081,0x00 Reg = 0,0x0082,0x00 Reg = 0,0x0083,0x00 Reg = 0,0x0084,0x00 Reg = 0,0x0090,0x00 Reg = 0,0x0091,0x00 Reg = 0,0x0092,0x00 Reg = 0,0x0093,0x00 Reg = 0,0x0094,0x00 Reg = 0,0x0098,0x00 Reg = 0,0x0099,0x00 Reg = 0,0x009A,0x00 Reg = 0,0x009B,0x00 Reg = 0,0x009C,0x00 Reg = 0,0x009D,0x00 Reg = 0,0x009E,0x00 Reg = 0,0x009F,0x00 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x00 Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C4,0x00 Reg = 0,0x00C5,0x00 Reg = 0,0x00C8,0x00 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0x00 Reg = 0,0x00E3,0x00 Reg = 0,0x00E8,0x00 Reg = 0,0x00E9,0x00 Reg = 0,0x00EA,0x00 Reg = 0,0x00F0,0x00 Reg = 0,0x00F1,0x00 Reg = 0,0x00F2,0x00 Reg = 0,0x00F3,0x00 Reg = 0,0x00F4,0x00 Reg = 0,0x00F5,0x00 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
[REGISTERS] Device = ALP Nano 1 - DS90UH949, Connector 1 Comments = "1234" Date = 04/06/2020 Time = 16:47:35 Reg = 0,0x0000,0x24 Reg = 0,0x0001,0x00 Reg = 0,0x0003,0x08 Reg = 0,0x0004,0x80 Reg = 0,0x0005,0x00 Reg = 0,0x0006,0x58 Reg = 0,0x0007,0x00 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x3F Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x03 Reg = 0,0x000D,0x20 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x88 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x01 Reg = 0,0x0016,0xFE Reg = 0,0x0017,0x1E Reg = 0,0x0018,0x7F Reg = 0,0x0019,0x7F Reg = 0,0x001A,0x01 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x00 Reg = 0,0x001D,0x00 Reg = 0,0x001E,0x01 Reg = 0,0x001F,0x00 Reg = 0,0x0020,0x0B Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x25 Reg = 0,0x0023,0x00 Reg = 0,0x0024,0x00 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x00 Reg = 0,0x0027,0x00 Reg = 0,0x0028,0x01 Reg = 0,0x0029,0x20 Reg = 0,0x002A,0x20 Reg = 0,0x002B,0x98 Reg = 0,0x002C,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x00 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x00 Reg = 0,0x003D,0x00 Reg = 0,0x003E,0x00 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x14 Reg = 0,0x0041,0x4B Reg = 0,0x0042,0x00 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x80 Reg = 0,0x0045,0x00 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x00 Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x00 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x97 Reg = 0,0x0051,0xA1 Reg = 0,0x0052,0x1E Reg = 0,0x0053,0x00 Reg = 0,0x0054,0x20 Reg = 0,0x0055,0x0C Reg = 0,0x0056,0x2A Reg = 0,0x0057,0x00 Reg = 0,0x0058,0x00 Reg = 0,0x0059,0x00 Reg = 0,0x005A,0x1A Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x02 Reg = 0,0x005D,0x06 Reg = 0,0x005E,0x44 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x22 Reg = 0,0x0061,0x02 Reg = 0,0x0062,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x00 Reg = 0,0x0074,0x00 Reg = 0,0x0075,0x00 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x00 Reg = 0,0x007D,0x00 Reg = 0,0x0080,0xC2 Reg = 0,0x0081,0x35 Reg = 0,0x0082,0xC7 Reg = 0,0x0083,0x68 Reg = 0,0x0084,0xF2 Reg = 0,0x0090,0x9F Reg = 0,0x0091,0x2E Reg = 0,0x0092,0x66 Reg = 0,0x0093,0xF4 Reg = 0,0x0094,0x02 Reg = 0,0x0098,0xD4 Reg = 0,0x0099,0x26 Reg = 0,0x009A,0xC4 Reg = 0,0x009B,0x51 Reg = 0,0x009C,0x82 Reg = 0,0x009D,0x17 Reg = 0,0x009E,0x68 Reg = 0,0x009F,0xA0 Reg = 0,0x00A0,0x13 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x00 Reg = 0,0x00A3,0x00 Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C2,0xA8 Reg = 0,0x00C3,0x15 Reg = 0,0x00C4,0x09 Reg = 0,0x00C5,0x40 Reg = 0,0x00C6,0x00 Reg = 0,0x00C7,0x6A Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00CE,0xFF Reg = 0,0x00D0,0x00 Reg = 0,0x00D1,0x00 Reg = 0,0x00D2,0x00 Reg = 0,0x00D3,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0xA8 Reg = 0,0x00E3,0x15 Reg = 0,0x00E4,0x09 Reg = 0,0x00E5,0x78 Reg = 0,0x00E6,0x00 Reg = 0,0x00E7,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x48 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x39 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
symptom 2: DS90UH949 had detected the HDMI clock, however the processor no display. Pull the HPD pin of DS90UH949 it can recover.
DS90UH949 and DS90UH940 register dump as below
[REGISTERS] Device = ALP Nano 1 - DS90UH949, Connector 1 Comments = "1234" Date = 04/06/2020 Time = 17:24:23 Reg = 0,0x0000,0x24 Reg = 0,0x0001,0x00 Reg = 0,0x0003,0xDA Reg = 0,0x0004,0x80 Reg = 0,0x0005,0x00 Reg = 0,0x0006,0x58 Reg = 0,0x0007,0x00 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0xC8 Reg = 0,0x000B,0x01 Reg = 0,0x000C,0x07 Reg = 0,0x000D,0x20 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x88 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x01 Reg = 0,0x0016,0xFE Reg = 0,0x0017,0x1E Reg = 0,0x0018,0x7F Reg = 0,0x0019,0x7F Reg = 0,0x001A,0x01 Reg = 0,0x001B,0x00 Reg = 0,0x001C,0x00 Reg = 0,0x001D,0x00 Reg = 0,0x001E,0x01 Reg = 0,0x001F,0xF6 Reg = 0,0x0020,0x0B Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x25 Reg = 0,0x0023,0x00 Reg = 0,0x0024,0x00 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x00 Reg = 0,0x0027,0x00 Reg = 0,0x0028,0x01 Reg = 0,0x0029,0x20 Reg = 0,0x002A,0x20 Reg = 0,0x002B,0x90 Reg = 0,0x002C,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x00 Reg = 0,0x0033,0x00 Reg = 0,0x0034,0x00 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x00 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x00 Reg = 0,0x003D,0x00 Reg = 0,0x003E,0x00 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x14 Reg = 0,0x0041,0x4B Reg = 0,0x0042,0x00 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x80 Reg = 0,0x0045,0x00 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x00 Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x00 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x00 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x97 Reg = 0,0x0051,0xA1 Reg = 0,0x0052,0x1E Reg = 0,0x0053,0x00 Reg = 0,0x0054,0x20 Reg = 0,0x0055,0x0C Reg = 0,0x0056,0x3F Reg = 0,0x0057,0x00 Reg = 0,0x0058,0x00 Reg = 0,0x0059,0x00 Reg = 0,0x005A,0xCD Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x02 Reg = 0,0x005D,0x06 Reg = 0,0x005E,0x44 Reg = 0,0x005F,0x4A Reg = 0,0x0060,0x22 Reg = 0,0x0061,0x02 Reg = 0,0x0062,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x00 Reg = 0,0x0074,0x00 Reg = 0,0x0075,0x00 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x00 Reg = 0,0x007C,0x00 Reg = 0,0x007D,0x00 Reg = 0,0x0080,0xC2 Reg = 0,0x0081,0x35 Reg = 0,0x0082,0xC7 Reg = 0,0x0083,0x68 Reg = 0,0x0084,0xF2 Reg = 0,0x0090,0x9F Reg = 0,0x0091,0x2E Reg = 0,0x0092,0x66 Reg = 0,0x0093,0xF4 Reg = 0,0x0094,0x02 Reg = 0,0x0098,0x9E Reg = 0,0x0099,0x0B Reg = 0,0x009A,0xE6 Reg = 0,0x009B,0x76 Reg = 0,0x009C,0x21 Reg = 0,0x009D,0xBD Reg = 0,0x009E,0x65 Reg = 0,0x009F,0xA9 Reg = 0,0x00A0,0x13 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x00 Reg = 0,0x00A3,0x00 Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C2,0xA8 Reg = 0,0x00C3,0x15 Reg = 0,0x00C4,0x29 Reg = 0,0x00C5,0x40 Reg = 0,0x00C6,0x00 Reg = 0,0x00C7,0x6E Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00CE,0xFF Reg = 0,0x00D0,0x00 Reg = 0,0x00D1,0x00 Reg = 0,0x00D2,0x00 Reg = 0,0x00D3,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0xA8 Reg = 0,0x00E3,0x15 Reg = 0,0x00E4,0x29 Reg = 0,0x00E5,0x78 Reg = 0,0x00E6,0x00 Reg = 0,0x00E7,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x48 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x39 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
[REGISTERS] Device = ALP Nano 1 - DS90UH940, Connector 1 Comments = "1234" Date = 04/06/2020 Time = 17:25:36 Reg = 0,0x0000,0x58 Reg = 0,0x0001,0x04 Reg = 0,0x0002,0x00 Reg = 0,0x0003,0xF0 Reg = 0,0x0004,0xFE Reg = 0,0x0005,0x1E Reg = 0,0x0006,0x00 Reg = 0,0x0007,0x24 Reg = 0,0x0008,0x00 Reg = 0,0x0009,0x00 Reg = 0,0x000A,0x00 Reg = 0,0x000B,0x00 Reg = 0,0x000C,0x00 Reg = 0,0x000D,0x00 Reg = 0,0x000E,0x00 Reg = 0,0x000F,0x00 Reg = 0,0x0010,0x00 Reg = 0,0x0011,0x00 Reg = 0,0x0012,0x00 Reg = 0,0x0013,0x00 Reg = 0,0x0014,0x00 Reg = 0,0x0015,0x00 Reg = 0,0x0016,0x00 Reg = 0,0x0017,0x00 Reg = 0,0x0018,0x00 Reg = 0,0x0019,0x01 Reg = 0,0x001A,0x00 Reg = 0,0x001B,0xF5 Reg = 0,0x001C,0x3B Reg = 0,0x001D,0x40 Reg = 0,0x001E,0x00 Reg = 0,0x001F,0x00 Reg = 0,0x0020,0x00 Reg = 0,0x0021,0x00 Reg = 0,0x0022,0x00 Reg = 0,0x0023,0x20 Reg = 0,0x0024,0x08 Reg = 0,0x0025,0x00 Reg = 0,0x0026,0x83 Reg = 0,0x0027,0x84 Reg = 0,0x0028,0x11 Reg = 0,0x0029,0x00 Reg = 0,0x002A,0x00 Reg = 0,0x002B,0x00 Reg = 0,0x002C,0x00 Reg = 0,0x002D,0x00 Reg = 0,0x002E,0x00 Reg = 0,0x002F,0x00 Reg = 0,0x0030,0x00 Reg = 0,0x0031,0x00 Reg = 0,0x0032,0x90 Reg = 0,0x0033,0x25 Reg = 0,0x0034,0x01 Reg = 0,0x0035,0x00 Reg = 0,0x0036,0x00 Reg = 0,0x0037,0x88 Reg = 0,0x0038,0x00 Reg = 0,0x0039,0x00 Reg = 0,0x003A,0x00 Reg = 0,0x003B,0x00 Reg = 0,0x003C,0x20 Reg = 0,0x003D,0xC0 Reg = 0,0x003E,0x23 Reg = 0,0x003F,0x00 Reg = 0,0x0040,0x43 Reg = 0,0x0041,0x03 Reg = 0,0x0042,0x03 Reg = 0,0x0043,0x00 Reg = 0,0x0044,0x60 Reg = 0,0x0045,0x88 Reg = 0,0x0046,0x00 Reg = 0,0x0047,0x00 Reg = 0,0x0048,0x0F Reg = 0,0x0049,0x00 Reg = 0,0x004A,0x00 Reg = 0,0x004B,0x08 Reg = 0,0x004C,0x00 Reg = 0,0x004D,0x00 Reg = 0,0x004E,0x63 Reg = 0,0x004F,0x00 Reg = 0,0x0050,0x03 Reg = 0,0x0051,0x10 Reg = 0,0x0052,0x00 Reg = 0,0x0053,0x01 Reg = 0,0x0054,0x80 Reg = 0,0x0055,0x00 Reg = 0,0x0056,0x00 Reg = 0,0x0057,0x00 Reg = 0,0x0059,0x7F Reg = 0,0x005A,0x20 Reg = 0,0x005B,0x20 Reg = 0,0x005C,0x00 Reg = 0,0x005D,0x00 Reg = 0,0x005F,0x00 Reg = 0,0x0060,0x00 Reg = 0,0x0061,0x00 Reg = 0,0x0062,0x00 Reg = 0,0x0063,0x00 Reg = 0,0x0064,0x10 Reg = 0,0x0065,0x00 Reg = 0,0x0066,0x00 Reg = 0,0x0067,0x00 Reg = 0,0x0068,0x00 Reg = 0,0x0069,0x00 Reg = 0,0x006A,0x00 Reg = 0,0x006B,0x00 Reg = 0,0x006C,0x00 Reg = 0,0x006D,0x04 Reg = 0,0x006E,0x00 Reg = 0,0x006F,0x00 Reg = 0,0x0070,0x00 Reg = 0,0x0071,0x00 Reg = 0,0x0072,0x00 Reg = 0,0x0073,0x07 Reg = 0,0x0074,0x07 Reg = 0,0x0075,0x08 Reg = 0,0x0076,0x00 Reg = 0,0x0077,0x00 Reg = 0,0x0078,0x00 Reg = 0,0x0079,0x00 Reg = 0,0x007A,0x00 Reg = 0,0x007B,0x5D Reg = 0,0x007C,0x02 Reg = 0,0x0080,0xC2 Reg = 0,0x0081,0x35 Reg = 0,0x0082,0xC7 Reg = 0,0x0083,0x68 Reg = 0,0x0084,0xF2 Reg = 0,0x0090,0x9F Reg = 0,0x0091,0x2E Reg = 0,0x0092,0x66 Reg = 0,0x0093,0xF4 Reg = 0,0x0094,0x02 Reg = 0,0x0098,0x9E Reg = 0,0x0099,0x0B Reg = 0,0x009A,0xE6 Reg = 0,0x009B,0x76 Reg = 0,0x009C,0x21 Reg = 0,0x009D,0xBD Reg = 0,0x009E,0x65 Reg = 0,0x009F,0xA9 Reg = 0,0x00A1,0x00 Reg = 0,0x00A2,0x8C Reg = 0,0x00C0,0x00 Reg = 0,0x00C1,0x00 Reg = 0,0x00C4,0x01 Reg = 0,0x00C5,0x00 Reg = 0,0x00C8,0xC0 Reg = 0,0x00C9,0x00 Reg = 0,0x00CA,0x00 Reg = 0,0x00CB,0x00 Reg = 0,0x00CC,0x00 Reg = 0,0x00E0,0x00 Reg = 0,0x00E1,0x00 Reg = 0,0x00E2,0x00 Reg = 0,0x00E3,0x00 Reg = 0,0x00E8,0x03 Reg = 0,0x00E9,0x00 Reg = 0,0x00EA,0x00 Reg = 0,0x00F0,0x5F Reg = 0,0x00F1,0x55 Reg = 0,0x00F2,0x48 Reg = 0,0x00F3,0x39 Reg = 0,0x00F4,0x34 Reg = 0,0x00F5,0x30 Reg = 0,0x00F6,0x00 Reg = 0,0x00F8,0x00 Reg = 0,0x00F9,0x00
Any idea what might happen?