Part Number: TPS65987DDJ
Hello , i could use some help with understanding the suggested flash memory for TPS65987DDJ.
Looking at the datasheet http://www.ti.com/lit/ds/symlink/tps65987ddj.pdf , there is a table (Table 21.) with flash memory part numbers.
In our product we would like to use the W25Q80JVSNIQ memory that is suggested. But the problem is that the flash can use dual or quad SPI,
in datasheet https://www.winbond.com/resource-files/w25q80jv%20spi%20revc%2008182016.pdf , there is a section on this.
As you can see, if the part number ends with "IQ" , the quad SPI pins are enabled. So the suggested flash W25Q80JVSNIQ is a quad SPI flash.
The problem starts when you look at the TPS65987DDJ datasheet and see that it only supports dual SPI. So the question is, where is the mistake ?
In TPS65987DDJ datasheet , that suggests the flash memory or in the W25Q80JV flash memory datasheet ?