Part Number: ESD401
Hello
can we use ESD401 protection diode on 5V power line that will carry not more than 50mA current.
Or please suggest 5V power line ESD and Surge protection with smallest possible size.
Regards,
Raghu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ESD401
Hello
can we use ESD401 protection diode on 5V power line that will carry not more than 50mA current.
Or please suggest 5V power line ESD and Surge protection with smallest possible size.
Regards,
Raghu
Hi Raghu,
The ESD401 device has a working voltage of 5.5V so it will be capable of protecting your power line. The ESD401 offers level 4 ESD protection in accordance to IEC61000-4-2 and surge protection for up to 4.5A per IEC61000-4-5. Additionally it also offers a low capacitance of 0.77pF making it capable to protect high speed data lines. The device is offered in the 0402 package to provide protection for small designs.
Let me know if you have any additional questions!
Best regards,
Andy Robles