Other Parts Discussed in Thread: SN65HVD234, ISO1050, ISOW7841, ISO7041
Hi,
My customer is looking for CAN trx 3.3V for e-mobility project.
speed max 1Mbps, no FD, Fault tolerant, the higher the better even though not primary concern. Application is cost sensitive.
Supply 3.3V.
I am looking for p2p CAN trx as below table
|
Non isolated |
Isolated version |
|
|
Pinout |
The same for the 2 versions |
The same for the 2 versions |
|
Alimentazione |
3,3V |
3,3V logic side and self supplied bus side |
Do you have any recommendations?
Many Thanks,
Antonio