This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS6126: Not easy to find the device when switching HD3SS6126EVM

Part Number: HD3SS6126

hi Sir,

My customer use HD3SS6126 to switch two host with one device.

power on no at no matter which host, the host can recognize the device. But if we switch the device after power on, the host cannot recognize the device. if no hub, it works correct. the cable between evm and hub is only 15cm. they already try 3 different hubs. 

Do you think that it's driving issue or others?

Also, they put the asic on the board similar with block diagram. It shows the same issues. So, i think that there may be something wrong.

BR,

frank