Part Number: DS90UB933-Q1
Do we have any information on how long it takes to go from; a digital change on parallel input serialized, passed over the FPD-LINK III, deserialized and then appear at the parallel output of a companion DS90UB934?
Also, can you clarify the spectrum that is used to transmit both the serialized channel and the bidirectional data channel? I can see a lot of talk about spread spectrum and that the bandwidth is max 100 MHz, but nothing about the centre frequencies.