This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: power consumption in specific condition

Part Number: DS90UB933-Q1

Hello, I need Maximum current of below condition. Can you provide (or estimate?)

933: 10bit mode, 72MHz, IDDT

934: 10bit mode, 72Mhz , IDD

These are needed to check if my load switch can handle the current. Right now I am calculating using datasheet value, but total current exceeds what the load switch can handle only a bit, and datasheet value should be a bit higher than my use case, so i am hoping that I could find path to meet current requirement.