Part Number: DP83822IF
Hello,
We are using the DP83822IF in our design. We can't get the media side link to come up. We tried the various loopback mode in the PHY and here are the results;
BIST and PCS Input Loopback, PRBS checker is locked and there is no error
BIST and PCS Output Loopback, PRBS checker is locked and there is no error
BIST and Digital Loopback, PRBS checker is locked and there is no error
We then proceeded to disable the loopback and used an external loopback plug. PRBS check is never locked or synced. I would presume that the receiver doesn't see the packet?
We also don't get the link up with the loopback plug. All the above were tried with auto-negotiation disabled and the speed set to 100M.
Below is the schematics of the media side connection. Requesting to review this section and let us know if there are any issues. Note we have used integrated magnetics with part number JX00-0027NL. The magnetics has the same specification as the recommended list in the datasheet.
Thanks in advance.
Vijay