Part Number: TPD6S300A
Team,
Customer tested on EVM and they dragged CC pin voltage to 5V to make OVP event, which could disconnect VBUS as an active protection function. But it seems like there are two different conditions in EVM. The first one didn’t retry and the second one is retry. May I know if it is depends on voltage threshold of VBUS?
Thanks a lot!!