This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83826E: LED driver and termination resistor questions.

Part Number: DP83826E

Hi All,

I feel really silly asking this, but I can't seem to find the answer in the data sheet.

Do the LED pins provide power to light the LED on the jack, or are they open-drain and rely on the other side of the LED being tied high through a current-limiting resistor?

Also:

There are termination resistors on the RX lines. Do you need to provide external 50 Ohm series resistors on the TX lines as well?

Do you need to tie the RX_D2 and RX_D3 lines low when using the chip in RMII mode?

Thanks

Glenn