Part Number: TUSB4041I
I'm using a TUSB4041I Eval board. I have a Samsung S9 phone as the upstream/host device, and I have a few peripherals plugged in via the TI USB Hub.
The setup works fine but I also need to charge the phone while using the peripheral USB devices. Fast charging is not a requirement. I will provide the 5V source to charge the phone.
I 've read that this is possible with Micro USB. You can tie the ID pin to ground with a 50k resistor and the phone will both act as a host AND receive a charge. But the Samsung S9 has USB-C which has no ID pin. Is this possible with USB-C?