Part Number: TIC10024-Q1
I presently monitor ground closure switches using a 10kΩ pull up to 5V and a Schmitt trigger input such as a 74LVX132 and aggregated using 74HC165s. Primarily to reduce board complexity, I am considering replacing this logic with a TIC10024-Q1.
I expect to operate in polling mode with 2mA wetting as more doesn't seem necessary. The "cleaning" capability is unlikely to be used. I am not constrained by "automotive" standards.
Given all of this, I'm struggling to understand the benefits of an external series resistor and/or capacitor to ground on a per-channel basis.
Questions:
- Given the circuit described works well today, is there, strictly speaking, any requirement for the RC network on each input as shown in the data sheet?
- If so, why?
- If not, it would seem that a higher threshold voltage (say, 4V vs 2V) is a better choice on first principles. Do you agree?
- If the inputs are instead closures to Vs, is there, strictly speaking, any requirement for the RC network?