Part Number: DS90UB924-Q1
Hi TI,
I have a question for TI 924 and 926.
I think, two ICs (924 and 926) is almost same.
what are the main differences for each ICs ?
When I choose 924 or 926, how can I choose better one ?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB924-Q1
Hi TI,
I have a question for TI 924 and 926.
I think, two ICs (924 and 926) is almost same.
what are the main differences for each ICs ?
When I choose 924 or 926, how can I choose better one ?
Thanks
Hello Minwoo,
The only difference between 926 and 924 is the maximum PCLK support. 926 supports up to 85MHz and 924 supports up to 96MHz. If your application can use 85MHz then 926 is more cost effective.
Best Regards,
Casey