Part Number: DP83867E
Hi,
There are DP83867E and KSZ9477 on My board, Via SGMII , KSZ9477 and DP83867E are connected .
Now I checked the power up voltage LED0\RX-CTRL\LED1,they are 0.45v,0.64v and 1.9v.
This means LED0 is in mode2, LED1 is in mode 4 and RX-ctrl is in mode 3.
But the problem is when i pluged a cat5 which connect PC and RJ45 from dp83867, the widows show a red cross, which means there no connect.
Hope quickly reply