Part Number: DP83867IR
Other Parts Discussed in Thread: DP83867IS
Question regarding the power sequence and the RESET_n pin.
It looks like the RESET_n pin has a weak pullup (9k ohms), but to which rail is this pulled up?
Is it pulled up to the VDDA2P5, VDDIO, or VDD1P0? (I am skipping VDD1P8, as this is only optional for three-supply mode)
I ask this because the DS says for two-supply mode there is no recommendation on which power supply is ramped first/second, or how much delay there is between the two rails ramping. Yet there could be a situation where the RESET_n pin goes high while the voltages are still ramping, maybe causing some issues?
The engineer I am talking to believes the VDD1P0 rail needs to go high before, or at the same time, the RESET_n pin goes High. Is this understanding correct?
Also, is this true for DP83867IS device as well?
Thanks & Regards,
Darren