Part Number: TCAN1043-Q1
What happens to TCAN1043-Q1 if there is no series resistor on the WAKE input terminal and 12V is directly applied?
Thanks
Viktorija
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1043-Q1
What happens to TCAN1043-Q1 if there is no series resistor on the WAKE input terminal and 12V is directly applied?
Thanks
Viktorija
Viktorija,
The series resistance is meant to protect the WAKE pin against in-rush current when using a low-side/high-side switch to toggle the state of the pin for local wake-up. If the pin is constant tied to VBAT, there is no need for a series resistor to protect against potential damage.
Please let me know if you have any other questions.
Regards,
Eric, thanks.
In the instances where customer didn’t always have a constant 12V battery applied and instead it was ignition from the vehicle. Would we have issues with the transceiver? If so, what types of failure modes would we see? Would it be a total loss of the transceiver? Would only the LWU functionality be destroyed?
Viktorija,
Do you mean ignition as a switch for the battery to apply to WAKE? Or the supply to the entire transceiver and the WAKE pin at the same time?
If it's the former, this may cause issues and I would expect issues just with the WAKE function and pin. With a voltage applied to WAKE more current would be sunk by the pin because a lower-impedance path to GND would be created with the damage.
Regards,
Eric Hackett
Are either of these cases an issue?