Part Number: DS90UB953-Q1
Hi Expert
Could you please support my customers questions as below?
Q1, In order to consider the wiring of the line pattern of MIPI CSI-2, please tell the wiring length in the IC Package of each applicable pins.
Q2, Regarding the datasheet spec of Return Loss, S11=-20dB@1/2fBCC < f < 0.1GHz, -12dB@1GHz < f <fFC and something.(datasheet p72)
Is this spec for between the serializer(or deserializer) and the connecter? or between the serializer to the deserializer?
Customer understanding is, it is for between the serializer(or deserializer) and the connecter. is it correct?
Also, could you please provide me the information of the "Return Loss" + the "Insertion Loss"?
Q3, Regarding the SPEC of Insertion Loss for low frequency, it is -0.35dB@f <0.5GHz.
What is minimum frequency that should keep over -0.35dB performance?
From the FPD-Link III bandwidth (20MHz to 2.1GHz), is it okay to regard it as -0.35dB@20MHz <f <500MHz?
Q4, Does the DS90UB953-Q1 have the ASIL B, QM standard?
Thanks
Muk