Part Number: DS90UB947-Q1
Hi Team,
I read the 947 datasheet and face some questions showing as below.
--------------------------------
Single pixel openLDI interface means using D[3:0] input
Dual pixel openLDI interface means using D[7:0] input
Is above explanation right?
---------------------------------
If I use D[7:0] input openLDI and the deserializer output is D[7:0] fix, could output D[3:0] only?
If I use D[3:0] input openLDI and the deserializer output is D[3:0] fix, could output D[7:0] ?
---------------------------------
Regards,
Roy