Part Number: DS25BR110
Hi,
My customer has questions for Vth and Vtl. Datasheet show as below:
1. What kinds of condition is cause validation for +/- 100mV? e.g. high temperature condition? High/low voltage condition?
2. Customer confirmed DS25BR110 can detect 4 type of signals. But which signal can device support and which signal cannot device support in attached document?
3. If ambient temp is 10~40 degreeC, will the differential input range be small rather than +/-100mV?
4. Is there specific guild line to detect Rin(Input Termination Resistor)?
Regards,
Nagata.