Part Number: TUSB2036
I have a customer asking about settings for the following implementation. (Checked DS and EVM documentation)
Like in the below image, they want to implement this HUB so that a HOST(PC) can communicate directly to two MCUs.
They want the PC to be able to select which MCU (USB Transceiver, DP/DM) to communicate with, then only communicate between those devices.
What are the guidelines / settings needed to implement this? Is this just based on the VID / PID settings? EEPROM? Is there an APP note, or anything?