Part Number: DP83867ERGZ-R-EVM
Hi,
We use DP83867ERGZT ,the datasheet say
1.8-V Analog Supply (±5%).
No external supply is required for this pin. When unused, no connections
should be made to this pin.
For additional power savings, an external 1.8-V supply can be connected to
these pins. When using an external supply, each pin requires a 1-μF and 0.1-
μF capacitor to GND.
I want to know the meaning of power saving . 1.8V pin no connection or external supply connect,witch way is Recommended