Part Number: TPS25832-Q1
Hello,
We want to use the TPS25832-Q1 most time for connecting USB-Sensors to a custom processor board. It is implemented as USB-C lite, because only USB 2.0 lines are connected.
So it is an USB 2.0 connection in an USB-Type C connector. (Case 2).
But we also want to use the part to boot and flash our processor from a computer connected with USB Cable. (Case 1).
Is this possible with this part?
I have seen following in datasheet:
"The TPS2583x-Q1 is a Type-C controller that supports all Type-C functions in a downstream facing port"
In my case 1, it has to be an upstream facing port I think. So this wil not work?
Thanks for any help.
Dani