Part Number: DS90UB954-Q1
Hi there,
i have a question related to the synchronization between two different types of serializers using the same framesync signal generated internally on the TI954.
is it possible to generate a framesync signal on the TI954 side and send it/share it with both TI913A and TI935 and get them both synchronized on a frame level or the synchronization signal will be altered/adapted depending on the BC frequency. if the framesync is altered, is there another way to do it to keep them synced?
thank you and best regards,
omar