Part Number: TCA9617A
Other Parts Discussed in Thread: PCA9306, TCA9803, TCA9509
Hi TI Expert,
We have a problem with an I2C level conversion application, as shown in the following diagram.
PORT B of TCA9617, the output low-level voltage is 540mv, then via tca9548, PCA9306, the low-level voltage is still 540mv. Here,the I2C of PEX8796 is 1.8v interface, low level threshold is 630mv, the margin of 90mv is not enough.
We tried TCA9803 instead of TCA9617, and the PORT B of TCA9803 output low level 220mv. The low level voltage is more suitable, but there are many restrictions.
The two devices of TCA9548 and PCA9306 cannot be used together with TCA9803, and the function is not stable in the actual test.
Can you find a solution of p2p device to solve our problem?
BTW, Replace one of the TCA9617 with TCA9509, In this way, port A of TA9617 will be connected to port A of TCA9509. Is there any problem?
TCA9509 maybe not suitable for this, cause there is a description in datasheet 10.2.1 chapter.