Other Parts Discussed in Thread: DS90C3201, TFP401A, DS90C387A, TFP401, DS90C187, DS90C387
Hello,
I'm currently designing a monitor solution for HDMI/DVI (no audio). I would have to support both 1280x800 pixel single-link LVDS display and 1920x1080 pixel dual-link LVDS display with the same electronics.
Since TI doesn't have single-chip solution, I was planning to use TFP401A for receiver and then DS90C3201 for LVDS serialization to display. For dual-link this seems quite straightforward, just connect TFP401A odd pixel outputs to DS90C3201 odd-pixel inputs and the same for even pixels. However, TFP401A uses even-pixel outputs in 1-pixel/clock mode, but DS90C3201 uses odd LVDS ports (odd-pixel TTL inputs). This would mean that I would need to design two different boards: one with direct odd-odd and even-even connection (dual-link) and one with even-odd connection (single-link). Have I understood the specifications correctly? Is there any way around this?
If I have understood correctly, DS90UB949/DS90UB948 combination might do what I'm looking for, but the ICs are much more expensive, you can get even single-chip Analog Devices ADV7613 HDMI to LVDS bridge with less.
Best regards,
/ Ville