Part Number: DP83867E
Hello,
Customer uses the Boardcom IC (which only support fixed 1000Mbps SGMII protocol) to connect DP83867 with 4wire SGMI mode. The application environment is as this: switch(which only support 1000Mbps sgmii)——>phy——>RJ45
By debugging, the PHY data rate is only 10Mbps, and switch and PHY can't link, the related registers are configured as following:
0x01 7949
0x02 2000
0x03 A231
0x04 01E1
0x05 0000
0x06 0064
0x07 2001
0x08 0000
0x09 1300
0x0f 3000
0x10 5C48
0x11 A802
0x12 0000
0x13 0044
0x14 29C7
So the customer likes to confirm if DP83867 supports fixed 1000Mbps SGMII with 4wire mode? Because the register 0X13 is 0044 which indicates the xGMII error.
Best regards
Kailyn