This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB1064: I want USB SS/DP from the USB_C (connected to a USB Device) and the muxed output to go to DP monitor and USB3 MicroB PC host

Part Number: TUSB1064


Hello,

I have a device that supports DP alt mode and it has the ability to route USB3 (10gbps) or DP out of the USB Type C connector.

This devices generates the DP content

I'm making a board that will do two things:

1. Allow a USB HOST PC to connect to the TUSB1064 SS downstream ports and enumerate the previously mentioned device as a USB device (connected to the TUSB1064 SS upstream ports)

2. Route the DP output of the TUSB1064 to a DP connector which will be connected to a DP monitor using a DP-DP cable

I think the DP port part is fine with the TUSB1064, but all the EVM documents I see reference connected a the downstream USB pins to devices / hubs and the upstream to the host PC, whereas I want the opposite.