Part Number: TUSB546A-DCI
Other Parts Discussed in Thread: TUSB564
Hi,
I want to use TUSB546 on a project.
USB3.1 + 2Lane DP+AUX Alt Mode in a Source Device.
Two questions;
1) If I used TUSB546 on the source side out, Do I have to use TUSB564 on the sink side?
A USB-C legacy monitor can be connected to my source board? Because it has no TUSB564 own.
Which mode should I use? Flip or No Flip mode? What is depend on?
If cable connected opposite side, TUSB546 device can be manage it by CC1&2 pins on a usb-c legacy monitor without any problem?
2) Seen PCB trace of length (Xcd) is 12inch in TUSB546 datasheet. Is it max. length? GPU (IMX8 MCU) and TUSB can be closer than it on PCB. Right?
Thanks.
Ali