Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869
We are making three designs based on the DP83869HM. We will use it in media converter applications both for 100 and 1000 Mbps and we are using only straps to configure. To differentiate between 100 and 1000M we have a switch to pull pin 22 (JTAG_TDO/GPIO_1) either up or down. We strap down pin 45 & 46 (LED_1 & _2) to set copper AN to 10/100 and 100/1000 depending on if 100 or 1000 mode is set. We have the following customer requirements:
1. Link loss pass through, solved by pulling pin 32 (RX_CLK) down
2. Fiber force mode, solved by strap pin 47 (LED_0) up to disable fiber auto-negotiation (802.3 clause 37)
3. Non-transparent mode, i.e. copper interface auto-negotiation depends on the fiber side.
I am unsure how to solve the 3rd requirement. I have noted the text "Copper interface will support auto-negotiation, but the user will have to ensure that the speed negotiated on the copper side matches the speed fixed on the fiber side. In cases of speed mismatch between copper and fiber, interface data transmission will not be successful." in section 9.4.7 in the data sheet but is unsure what that means for this application where we have FULL control that device attached to the copper side supports the selected fiber speed and that the TP cable that connects the device to the media converter is a sufficiently good cable (typically 25 cm Cat5e not changeable by the user). I.e. if the device on the copper side supports 100M and we have fixed the fiber to 100M, will we "always" get a 100M link? And the same question for 1000M?
I also need an answer to the formal question if the DP83869HM supports non-transparent mode. Does it support that? If the answer is NO, which IC would you propose for us to use instead?