Part Number: DS90UB953A-Q1
Can I use such a chain to increase the length of the cable FPD-link III.
CSI-2 camera «---» Ser «---15m---»Des+Ser«---15m---».....«---15m---»Des«---» Processors
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953A-Q1
Can I use such a chain to increase the length of the cable FPD-link III.
CSI-2 camera «---» Ser «---15m---»Des+Ser«---15m---».....«---15m---»Des«---» Processors
Hello,
For 953 + 954/960 applications this can be done. It would not be suitable for all FPD-Link parts but since 953/954/960 for example use fixed frequency FPD-Link communications which are not derived from the input data clock, they will not accumulate jitter so this topology is supported.
Best Regards,
Casey
Thanks for the info.
Do I understand correctly that all 953 should work in Non-Synchronous Internal Mode?
Can I count on a stable throughput of 50 MHz * 80 = 4 Gbps in this case?
Hello,
Yes non-synchronous mode with internal clock is a supported mode for 953 @ 4Gbps forward channel rate.
Best Regards,
Casey