Part Number: TVS3300
Other Parts Discussed in Thread: CSD18510Q5B, LM74700-Q1, , TVS3301
I am planning on using a TI LM74700-Q1 ideal diode controller to control a TI CSD18510Q5B power MOSFET to protect a PCB with up to 28V input, at up to 15A continuous, 20A peak (or thereabouts...). The power source will typically be 6S LiPos with high C ratings, so they can deliver quite a jolt.
Reading the TI LM74700-Q1 datasheet, it seems the Littelfuse SMBJ33CA is an appropriate TVS diode to protect this PCB against power surges in the above-described system.
Is the TI TVS3300 an adequate substitute for the Littelfuse SMBJ33CA for such an application? Any benefits or concerns with this choice? The DSBGA version is adorably compact...