Part Number: SN65HVD235
Hello team,
My customer has been using SN65HVD235 CAN driver in their design for years. They have not had ESD issues in the past, however now they’re getting some hard and soft failures. Some times it fails and burns out the CPU port. On the soft fail something in the protection fails and it draws 30-40 mA more current. The outputs still function, but the IC gets hot. The part is rated to +/-15kV and the customer is testing at +/- 8kV. They have additional clamping on the ports from a PESD2IVN27-UX TVS part. This is the only port failing. Has something changed in the device? This is causing a lot of trouble passing certifications. Also, I have partial schematics that I can send internally if needed.
Thank you in advance for your support!
Errol