Part Number: TPS65987D
Hello,
I have a question about the current draw for the TPS65987D. Looking at the datasheet says IVIN_3V3 is typically 8mA when active. However, most of the EVMs and designs I've seen with the TPS65987D use a 1A - 3A power supplies. So I want to double check to see if I can use a 200 - 300mA LDO or do I need more current?
Thank you
Albert Lo