This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Minimum pulse width for external frame sync

Part Number: DS90UB954-Q1

Hello,

I'm using 954 EVB and 953 which is on our device.

All 4 GPIO are assigned.

ExternalSync is attached to GPIO0.

The FrameSync configuration of 954 was done according to the datasheet so:

FS_CTL 0x18 is 0x80

BC_GPIO_CTL0 0x6E is 0xA

1. What is the minimum pulse width that has to be configured at the 954 side?

In addition, I would like to transmit frame sync when the source is the device itself (the device synchronize other devices). In that case, the 953 GPIO is input and 954 is output.

2. What is the minimum pulse width that has to be configured at the 953 side (back channel)?